When ATS maintenance or testing is about to occur, ATS devices can be set to Ignore status. The platform will then bypass the ATS for four hours. During this time the platform will not send any alarms nor log data for that ATS.
Setting ATS to Maintenance Mode
-
While in ATS Entity Details, click Ignore. The platform will display ask for confirmation. Click OK.
-
The platform starts the 4:00:00 hour timer. After this timer finishes, the ATS should return to a normal status.
-
If the maintenance is completed before the timer has expired, select the X button to cancel the maintenance cycle. The timer will clear and status will return to normal.