On-Prem Knowledge Base

Aurora Application Programming Interface (API)

Using API Filters

The API exists as an endpoint on the Aurora Server and enables the retrieval of live and historical data by filter or individual tag. A filter can be created in Aurora by grouping a set of tags together for retrieval through the API.

Each filter is limited to 40 tags. If you need a filter with more than 40 tags, please contact Support.

Setting Up a Filter

  1. Open the Trending tab.

  2. Select a Date-Time range.

  3. Select a tag by clicking in the tag row. Once selected, Aurora On-prem will display the tag in the blank window.

API-tags-Range.jpg
All Available Tags by Date Range

Column headers have filter options so that the list of tags can be relevant to the need. For example, the user can filter by Site, System, Entity, and so on.

  1. Repeat step 2 until you have selected all the desired tags for the API Filter.

Tags-ATS.jpg
Populating the Selection Window
  1. Type a Filter Name in the Save Tag Selection field.

  2. Click Save; The API Filter is now available for use.

Save-Tag-Selectn.jpg
Naming and Saving Tag Selection

API Filters must be setup on each individual server.

API Authentication

The API uses basic authentication consisting of a user name and password. It is suggested that a user is created in Aurora specifically for API use and granted access to all systems containing tags that will be retrieved through the API.

Setup a Header with Basic Authentication

  1. Build a string of the form username:password.

  2. Base64 encode the string.

  3. Supply an “Authorization” header with content “Basic ” followed by the encoded string.

  4. For example, a user name of “test” with a password of “test” would be test:test which is dGVzdDp0ZXN0 after encoding. The request header should contain “Authorization: Basic dGVzdDp0ZXN0”.

API Methods

API calls are defined and highlighted in the table in this section.

Method

V1 Route

V2 Route

Description

GET

/v1/filters

/v2/filters

Gets Filters owned by authenticated user. Includes all associated tags and tag detail.

GET

/v1/filters/{filterId}/Historical

/v2/filters/{filterId}/Historical

Gets historical data for tags associated with the provided filter.

GET

/v1/filters/{filterId}/Live

/v2/filters/{filterId}/Live

Gets live data for tags associated with provided filter.

GET

/v1/tags/{tagId}/Historical

/v2/tags/{tagId}/Historical

Gets historical data for provided tag.

GET

/v1/tags/{tagId}/Live

/v2/tags/{tagId}/Live

Gets live data for the provided tag.

POST

/v1/tags/{tagId}?value={tvalue}

/v2/tags/{tagId}?value={tvalue}

Attempts to update value for provided tag.

POST

/v1/tags/Historical

/v2/tags/Historical

Allows insert of data to telemetry tables for Minute, QuarterHour, Hour, and Day for one or more existing tags.

GET

/v1/alarms

/v2/alarms

Returns list of current alarms.

GET

/v1/alarms/{alarmId}

/v2/alarms/{alarmId}

Returns current state for provided alarm.

GET /filters

Description: Gets Filters owned by the authenticated user. Includes all associated tags and tag detail.

Parameters: None

Supported Types: application/json

Sample Request: GET ../API/v1/filters

Responses: A successful request will return a HTTP status code of 200 and a response containing a filters object. See the Error Codes and Responses section for a full list of HTTP status and error codes.

GET /filters/{filterId}/Historical

Description: Gets historical data for the tags associated with the provided filter.

Parameters: Refer to the table in this section.

Name

Located In

Description

Required

FilterId

Path

id of filter containing list of tags to return.

Yes

Interval

Query string

Interval of data to be returned. Valid values are “Minute”, “QuarterHour”, “Hour”, and “Day”.

Yes

Start

Query string

Starting date/time range of data to retrieve.

Yes

End

Query string

Ending date/time range of data to retrieve.

Yes

DateRangeType

Query string

Identifies time zone to use when applying the Start and End date range. Valid values are “UTC” and “Site”. If not set, default is “Site”.

No

Supported Types

  • application/json

  • text/csv

Sample Request

GET ../API/v1/filters/{filterId}/Historical?Interval=QuarterHour&DateRangeType=Site&Start=2016-07-26

01:00:00&End=2016-07-27 01:00:00

Responses: A successful request will return a HTTP status code of 200 and a response containing a historical data object. See the Error Codes and Responses section for a full list of HTTP status codes and error codes.

GET /filters/{filterId}/Live

Description: Gets live data for the tags associated with the provided filter.

Parameters: Refer to the table in this section.

Name

Located In

Description

Required

FilterId

Path

id of filter containing list of tags to return.

Yes

Supported Types: application/json

Sample Request: GET ../API/v1/filters/{filterId}/Live

Responses: A successful request will return a HTTP status code of 200 and a response containing a live data object. See the Error Codes and Responses section for a full list of HTTP status codes and error codes.

GET /tags/{tagId}/Historical

Description: Gets historical data for the provided tag.

Parameters: Refer to the table in this section.

Name

Located In

Description

Required

TagId

Path

The id of the tag to return.

Yes

Interval

Query string

Interval of data to be returned. Valid values are “Minute”, “QuarterHour”, “Hour”, and “Day”.

Yes

Start

Query string

Start date/time of data to retrieve.

Yes

End

Query string

End date/time range of data to retrieve.

Yes

DateRangeType

Query string

Identifies the timezone to use when applying Start and End dates. Valid values are “UTC” and “Site”. If not set, default is “Site”.

No

Supported Types

  • application/json

  • text/csv

Sample Request

GET ../API/v1/tags/{tagId}/Historical?Interval=QuarterHour&DateRangeType=Site&Start=2016-07-2601:00:00&End=2016-07-27 01:00:00

Responses: A successful request will return a HTTP status code of 200 and a response containing a historical data object. See the Error Codes and Responses section for a full list of HTTP status codes and error codes.

GET /tags/{tagId}/Live

Description: Gets live data for the provided tag.

Parameters: Refer to the table in this section.

Name

Located In

Description

Required

TagId

Path

id of tag to return.

Yes

Supported Types: application/json

Sample Request: GET ../API/v1/tags/{tagId}/Live

Responses: A successful request will return a HTTP status code of 200 and a response containing a live data object. See the Error Codes and Responses topic for a full list of HTTP status codes and error codes.

POST /tags/{tagid}?value={value}

Description: Attempts to update value for the provided tag.

Parameters: Refer to the table in this section.

Name

Located In

Description

Required

TagId

Path

The id of tag to write a value against.

Yes

Value

Query string

Value to write. This must match the defined tag type. So if the tag is a discrete type, the value must be true or false, otherwise, numeric.

NOTE: If there’s a configured range for the tag, the value must be within the range or an error will be returned.

Yes

Supported Types: application/json

Sample Request: POST ../api/v1/tags/{tagid}?value={value}

Responses: A successful request will return a HTTP status code of 200. See the Error Codes and Responses section for a full list of HTTP status codes and error codes.

Post /v1/tags/Historical

Description: Allows insert of data to our telemetry tables for Minute, QuarterHour, Hour and Day for one or more existing tags.

Parameters: None

Supported Types: application/json

Sample Request: POST ../api/v1/historical

Request Body: Accepts historical data object.

Responses: A successful request will return a HTTP status code of 200. See the Error Codes and Responses section for a full list of HTTP status codes and error codes.

Get /v1/alarms

Description: Returns a list of current alarms.

Parameters: None

Supported Types: application/json

Sample Request: GET ../api/v1/alarms

Responses: A successful request will return a HTTP status code of 200 and a response containing an alarm data object. See the Error Codes and Responses section for a full list of HTTP status codes and error codes.

Get /v1/alarms/{alarmid}

Description: Returns the current state for the provided alarm.

Parameters

Parameters: Refer to the table in this section.

Name

Located In

Description

Required

Alarmid

Path

The id of the alarm to retrieve.

No; If not supplied, all current alarms will be returned.

Supported Types: application/json

Sample Request: GET ../api/v1/alarms/{alarmid}

Responses: A successful request will return a HTTP status code of 200 and a response containing an alarm data object. See the Error Codes and Responses section for a full list of HTTP status codes and error codes.