From the EMPS screen, click the (+) Fuel Systems(s) adjacent to the section header to expand the fuel system displays in order to view details.
Click a line item in the Fuel Systems tree to open Fuel System details at the bottom of the page. Data provided includes capacity, total fuel, as well as time on hand.
Fuel System values are defined in the table in this section.
Fuel System Field Definitions
Field Indicator
|
Description
|
|---|---|
Status
|
|
System Time On Hand
|
Estimation of the amount of time fuel system can sustain ALL generators if they were to run at the present TOTAL load demand. |
|
Under Current Usage |
Estimation of the amount of time fuel system can sustain the generators that are presently running at current GENERATOR load demand. |
|
Fuel Gauge |
Represents the fuel level (gals) of all tanks combined. |
|
Total Capacity |
The fuel tank capacity for all tanks combined. |
|
Total Percent |
The percent of total fuel remaining. |
The purpose of time to empty and fuel level information is to help the user make optimal decisions regarding fuel availability and/or replacement. Fuel estimations are based on manufacturer specifications and available fuel system data.