Skip to main content
Skip table of contents

Operations Summary

The Operations Summary feature facilitates equipment monitoring and alarm activity by building, floor, and room.

To access the Operations Summary:

  1. Select the Operations menu option.

  2. Select Summary from the menu list so that the platform displays the Operations Summary.

image-20240612-163422.png

Operations: Summary

To collapse or expand sections of the screen use the (-) and (+) buttons next the section header or the Expand All/Collapse All options in the upper right-hand corner.

Ops_event_logs.jpg

Operations: Menu Selection

The Communication Status column indicates the number of assets that are both offline or online on the summary view.

OFFLINE

ONLINE

The Equipment Status column indicates the status of the equipment/asset.

ACTIVE

Running on generator power

INACTIVE

“Ready” and on utility power

NOT READY

Generator is in Not in Auto mode

IGNORE

ATS was put in Maintenance mode in Aurora

UKNOWN

Platform is uncertain of status

The Alarm column provides the following alarm status values. Parenthesis indicate the

ALARMS (0)

No Alarms

ALARMS (1)

Active Alarms

ALARMS (1)

Not an active alarm, however it is unacknowledged.

Equipment Details

Click into the equipment row on the Operations Summary so that the platform will display equipment values.

image-20240612-164620.png

Equipment Details

JavaScript errors detected

Please note, these errors can depend on your browser setup.

If this problem persists, please contact our support.